When deploying laptop locks, balancing individual access for employees while simplifying key management can be a complex and time-consuming process. There are two approaches for keyed locks that can make device security easier to manage: Master Keyed and Keyed Alike. Learn more about these two options for keyed locks, both now available in convenient multi-packs that simplify large scale deployments. Master Key Approach This option provides unique keys for each lock and an optional master key for administrators, along with universal compatibility and scalability. 25 Pack Master Key Locks UNIVMK25-LAPTOP-LOCK Keyed Alike Approach With this option, one key is used to access multiple locks, simplifying device security without the hassle of managing multiple keys or combinations. 25 Pack Keyed Alike Locks UNIVKA25-LAPTOP-LOCK Master Key Option IT departments often balance the need to grant individual access to employees while maintaining a simplified method for unlocking any lock in case of misplaced keys, lock repurposing, or employee departures. Here’s how it works: Unique Keys for Each Lock: A unique key is provided for every lock, allowing each user to unlock and relocate their equipment as needed. Optional Master Key: An IT administrator or designated keyholder has the flexibility of ordering an optional master key. This master key grants access to all locked hardware without requiring physical key management for individual locks. Universal Compatibility: Master Key locks are universally compatible with K-Slot, nano K-Slot, and Noble Wedge devices, ensuring a broad range of devices used within an organization can be secured. A Lock selection dial enables quick selection of the required lock tip without disassembly or additional adapters that can be misplaced. Scalability: Available in convenient 25-packs, these locks are ideal for larger deployments. Additional units can be ordered as needed for new team members or devices. Master Keyed locks provide a practical solution for IT managers, combining security with flexibility. By simplifying key management and ensuring individual access, organizations can enhance efficiency and streamline their security. Keyed Alike Option Newly deployed hardware, such as laptops, docks and monitors on shared desks, often requires secure locking. Managing multiple keys can become cumbersome, especially when only the IT department or an Administrator requires access. The challenge lies in finding a solution that balances security with ease of use. Enter keyed alike locks: a smart solution that offers flexibility and efficiency. One Key, Multiple Locks: Keyed alike locks allow office assets to be secured without juggling a bunch of keys. With one key, an Administrator can access multiple locks. Temporary Locking Made Easy: These locks let you temporarily secure devices at workstations without the hassle of managing different keys or remembering various combinations. Exclusive Access: Each 25-pack of keyed alike locks includes two pairs of keys. The IT department or a designated key holder can enjoy exclusive access, ensuring security when users access is not required or should be restricted. Universal Compatibility: Like Master Key locks, these keyed alike locks also work seamlessly with K-Slot, nano K-Slot, and Noble Wedge devices, utilizing a selection dial enables quick selection of the required lock tip without disassembly or additional adapters. As you can see, there are advantages to selecting either the Master Key or Keyed Alike approach for device security. Serialized combination and Dual Keyed and Combo Lock options are also available. Choose the right option based on your organization’s technology environment and the needs of your administrators and users. Serialized combination locks are another alternative to keyed options and offer their own unique benefits. StarTech.com will be launching keyless combination locks, also available in convenient multipacks, in the near future. Download our Laptop Locks guide for more detailed information on the options available or learn more about each option at the links below. Also, look for our new combination lock options coming soon! Master Key Locks UNIVMK25-LAPTOP-LOCK Keyed Alike Locks UNIVKA25-LAPTOP-LOCK