Press releases

New StarTech.com GaN Charger Prevents Overheating While Delivering Peak Device Charging Performance

Groveport, OH – December 11th, 2024 – StarTech.com, the leading manufacturer of performance connectivity accessories for IT Professionals, announces the newest addition to its premium line of power adapters. The 140W USB-C GaN Wall Charger ensures consistent, peak power delivery for high-performance devices such as the newly released M4 Pro and Max MacBooks as well as M3 MacBooks, premium laptops and all other USB-C chargeable electronics.
 

Unlike other power adapters that are prone to overheating, the 140W GaN Wall Charger is engineered for cool performance under extended full load use, keeping the charger cool to the touch while providing consistent unthrottled power delivery. 

Built with device safety in mind, the USB-IF certified 140W charger also protects connected devices from over-voltage, over-heating, over-current and short circuits. The charger includes an extra-long 6 foot, 240W EPR rated, certified USB-C cable for added convenience. 


“Most people have felt the uncomfortable sting of unplugging an overheated charger at some point, but our Product Development team has taken steps to solve this problem,” says Product Manager Tony Parackal, “This charger is designed to provide an optimal continuous peak power delivery while ensuring user and device safety.”
 

GaN technology allows the 140W USB-C GaN Wall Charger to deliver its high power with a small form factor compared to other contemporary charging technologies making it an excellent solution for anyone seeking an efficient and effective power source for their high-performance devices. The 140W charger is an ideal choice for environments where user safety is key such as education, medical or public workplaces.  

StarTech.com also offers additional chargers for a variety of applications: 

•    100W 2x USB-C 2xUSB-A quick charging GaN charger 
•    60w USB-C wall charger 
•    30w USB-C portable GaN wall charger 

StarTech.com chargers are available through leading IT resellers and distributors including CDW, Amazon, Ingram Micro, TD SYNNEX, and D&H. 
 

About StarTech.com

StarTech.com manufactures a broad portfolio of connectivity accessories designed to meet the rigorous performance requirements of IT professionals including docking stations, display adapters, video and audio cables, network products, ergonomic furniture and mounts.

Founded in 1985, StarTech.com has operations in 26 markets worldwide across five continents. StarTech.com has been named a winner of Canada's Best Managed Companies by Deloitte for 14 consecutive years and was included in Financial Post's FP500 ranking of Canada's Top 500 companies based on revenue in 2022.

Back to top