Updated Guide Now Available⤵ Multi-Monitor Solutions For Apple M1 / M2 System Deployments Apple’s high-performance M1 chipset is the first designed specifically for the Mac, boasting 3 times higher performance per watt and the “world’s fastest integrated graphics in a personal computer”. It is the first of a family of processors that Apple® will use in its Mac lineup. In 2020, the MacBook Pro 13, MacBook Air, and Mac Mini have been upgraded with the M1 chip with plans to transition every Mac model to an Apple Silicon by 2022. The Apple M1 chip is compatible with many of StarTech.com’s Docking Stations, Multiport Adapters, Display Adapters, and PCIe Expansion Chassis. Our Thunderbolt™ 3 and USB-C® products will provide full functionality such as laptop charging (via Power Delivery), audio, gigabit Ethernet, USB and storage devices. While the new Apple CPU silicon offers many high-performance features, including up to 6K support on a single extended display, there is a limitation of the M1 chipset with regards to extended multi-display support on Thunderbolt™ 3 interfaces. This means you can only connect one extended display from your Apple M1 MacBook Pro / Air. This impacts all Docking Stations and Thunderbolt™ 3 Display Adapters currently in the market and is not a limitation of StarTech.com products. Apple® lists support for only one extended display in the technical specifications for video support on the M1 MacBook Pro 13”. MacBooks using the Intel processor will still continue to support dual extended displays on Thunderbolt™ 3 Docking Stations and Display Adapters. Docking Stations Display Adapters USB-C MULTIPORT ADAPTERS USB-C DISPLAYLINK DOCKS Maximum Extended Displays 1 1 1 2 or 3 (Depending on Model) Maximum Mirrored Displays 2 2 1 2 or 3 (Depending on Model) Multi-Display Solution for M1-Based Mac Systems StarTech.com DisplayLink Docking Stations For those who require multiple extended displays while using an M1 chip-based MacBook, StarTech.com’s DisplayLink Docking Stations are a great alternative. Our DisplayLink docks not only support multiple displays on M1 based MacBooks, but they offer IT solutions with both dual and triple 4K 60Hz video outputs to optimize productivity. Use of DisplayLink docks will auto prompt the installation of Apple’s Rosetta 2 software if not already installed on your system. This software is needed in order to install the necessary DisplayLink drivers. StarTech.com DisplayLink docks come in a variety of port configurations to support your workstation connectivity requirements. DK30CH2DEP DK30C2DPEP DK30C2DPPD DK30CHDDPPD Video Output Ports 2xDisplayPort & 1xHDMI 2xDisplayPort & 2xHDMI 2xDisplayPort & 2xHDMI DisplayPort & HDMI Number of Displays 3 2 2 2 Maximum Resolution 4K 60Hz (DP) 4K 30Hz (HDMI) 4K 60Hz 4K 60Hz 4K 30Hz Power Delivery 100W 100W 60W 60W Downstream USB Ports 4x USB-A 1x USB-C 3x USB-A 1x USB-C 3x USB-A 1x USB-C 4x USB-A Downstream USB Speeds 5Gbps 5Gbps 5Gbps 5Gbps Ethernet 1 Gbps 1 Gbps 1 Gbps 1 Gbps Fast-Charge Yes Yes Yes Yes Other Downstream Ports 3x 3.5mm (Headset/Mic, line out, Mic in) 1x 3.5mm (Audio & Mic) 1x 3.5mm (Audio & Mic) SD Card Reader 1x 3.5mm (Audio & Mic, Headset) Apple® announces a new line of Mac computers featuring their new M1 Silicon Chip with plans to move all Macs to an Apple based Silicon by 2022. November 10th, 2020 Apple’s Press Release For any questions regarding this topic, please contact our Technical Advisors at StarTech.com/chat.