As a former IT Manager, and now in my current technical content role, I’ve thought extensively about both technology and security. With the continued prevalence of cloud-based computing and remote work, there are plenty of well-founded concerns related to software and network security specifically. Of course, those aspects are important but physical security also plays a critical role in business today. Recently I had the opportunity to talk with Ellard Teeple, our CTO, on the topic of security. We discussed several ways StarTech.com can help the IT Pro with security in the back office, front office, and on the road. Here’s the first of a two-part series discussing how we make computer security products easy to find. Foil prying eyes with monitor and laptop privacy screens. Prevent visual data from being compromised at workstations, or in public / high traffic areas, with the broad portfolio of privacy filters that support laptops, 2-in-1s, MacBooks, and desktop monitors in environments with new and legacy ecosystems. Built with advanced Microlouver technology to provide black-out privacy outside of the +/- 30 (60 total) degree viewing angle and maintain a high image clarity for the user, the filters feature a fingerprint, dust and scratch resistant coating. A protective sleeve is included to protect the filter when not in use, and filters are easy to clean using the included microfiber cloth. The reversible 2-in-1 filter has a matte side to eliminate reflections and glare for long hours of use, while glossy side provides added privacy with a quicker black-out transition and maintains contrast and color vibrancy. Reduce blue light transmission by up to 50% without compromising privacy while preventing eye strain! Keep portable devices safe by deploying flexible and secure user device locks. Designed for IT Pros to secure a mix of devices, Universal 3-in-1 locks support K-Slot, Nano, and Noble Wedge lock types. This can help secure all workstation peripherals using a single tether by using a laptop lock kit. Additional locks and anchor points can be added along the tether for a variety of devices such as laptops, monitors, docking stations, and projectors. A variety of lengths and styles are available. Increase security by having unique serialized keys or user resettable combination locks. Secure devices without a lock slot by using the Security Lock Slot Adapter Kit or use the Anchor for Cable Lock to secure multiple devices using a single cable. Designed with a protective spacer that prevents damage to the laptop, thin profile locks include a 90 degree elbow and 360 degree swivel to eliminate strain on ultra-slim devices. Securely attach docks and hubs to a monitor or stand with VESA mounting plates. A VESA Mount for Docking Stations / Hubs makes it easy to attach a compatible StarTech.com dock or hub to the backside of your monitor mounted on a stand or attached to a monitor arm with a VESA hole pattern. The sturdy and durable dock and hub mount is engineered from 10-gauge steel (3.3 mm thick). This mount provides a great way to free up desk space in offices in business or commercial spaces, and secure valuable IT equipment like a docking station. Also available in a Wall / Desk Mount version. Identify network devices while improving performance with connectivity tools software. StarTech.com Connectivity Tools is a free utility suite that can be downloaded to enhance the functionality of StarTech.com accessories like docks and adapters. IT Administrators can now easily identify, authorize, and track devices connected to your network, with features like MAC Address Pass-Through and USB Event Monitoring. Please watch our blog soon for the second part in this series where I’ll look at more security concerns we’re helping alleviate for IT Professionals and their users! In the meantime, check out this earlier post about 3 Unique IT Challenges Solved with Innovative Tech.